메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

What happen if data is executed without stopping prescaler and timer?

Latest Updated:03/04/2005

Question:

(Timer)   What will happen if the data read instruction is executed without stopping the counter for the programmable prescaler and timer? [2005/03/04]

Answer:

The counter value may not be read correctly. (#105065)
Suitable Products
4508
4509
4559
455A
4571
  • 이 기사가 도움이 되셨나요?