메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

What happen if data is executed without stopping programmable timer?

Latest Updated:02/05/2009

Question:

(Timer)  What will happen if the data read instruction is executed without stopping the counter for the programmable timer? [2009/02/05]

Answer:

The counter value may not be read correctly. (#107258)
Suitable Products
4286
  • 이 기사가 도움이 되셨나요?