메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

What happens if 0 is written in A/D converter completion bit when it is 0?

Latest Updated:03/01/2005

Question:

(A/D Converter)   What happens if "0" is written to the A/D converter completion bit when the bit is "0" (conversion in progess) ? [2005/03/01]

Answer:

If "0" is written to the A/D converter completion bit while the bit is "0" (conversion in progess), conversion will restart from the beginning. (#104832)
Suitable Products
3803H
3803L
3823
3850A
3858
38D2
38D5
7544
7546
7547
7548
7549
  • 이 기사가 도움이 되셨나요?