What happens if MSTP10 is set high during D/A conversion and its effect?
Latest Updated:03/23/2009
Question:
On the H8S/2328, what happens if MSTP10 is set High during D/A conversion and what is the effect on power consumption ?
Answer:
When the module stop bit is set, access to control registers is prohibited and the content of control registers and outputs are retained. The power consumption of the device will reduce, as in module stop the clock supply to corresponding module is removed.
Suitable Products