메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

What happens if the processor mode is change by setting it to bits?

Latest Updated:02/14/2006

Question:

When I change the processor mode by setting the processor mode bits, are the settings of the port register and port direction register maintained?

Answer:

Yes, the settings of the registers are maintained.
Suitable Products
M32C/8A
M32C/88
M32C/87
M32C/85
M32C/84
M32C/83
M32C/80
M16C/62A
M16C/62A(M16C/62T)
M16C/62M
M16C/62N
M16C/62N(M3062GF8NFP, M3062GF8NGP)
M16C/62P
M16C/63
M16C/64A
M16C/64C
M16C/65
M16C/65C
M16C/6C
M16C/6N4, M16C/6N5
M16C/6NK, M16C/6NL, M16C/6NM, M16C/6NN
  • 이 기사가 도움이 되셨나요?