메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

What is Internal Power Supply Generator (VDC)?

Latest Updated: 03/22/2017

Question:

What is an Internal Power Supply Generator?

Answer:

Internal Power Supply Generator (VDC) is a function that converts 5V and 3.3V, which are input to VCCER (main power supply) pin, to the voltage level for internal use.
Suitable Products
32185
32186
32192
32195
32196
  • 이 기사가 도움이 되셨나요?