메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

What is the characteristics of enhancement type of MOS FET?

Latest Updated:11/01/2005

Question:

What is the characteristics of enhancement type of MOS FET?

Answer:

This is a type of MOS FET. An enhancement type MOS FET has a characteristic that a drain current does not flow unless a gate voltage is applied. The gate voltage at which the drain current starts flowing is specified as a threshold voltage VT.
Today, enhancement type MOS FETs are generally used.

Suitable Products
  • 이 기사가 도움이 되셨나요?