메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

What is the contrast between complete version and simplified version?

Latest Updated:03/23/2017

Question:

It is stated that the IEBus controller is a "simplified version."
What is the difference between the complete version and the simplified version?
Also, is an external device required?

Answer:

The complete version of the IEBus controller has a 32-byte transmit/receive buffer, but the simplified version of the IEBus controller has only a 1-byte transmit/receive buffer.
An external differential driver is required on the transmit/receive data line (not manufactured by NEC Electronics).
Suitable Products
V850E2/Sx
V850E/Sx
V850ES/Sx
  • 이 기사가 도움이 되셨나요?