메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

What is the data in areas not programmed with FlashPro in uPD78F0034A?

Latest Updated:12/01/2011

Question:

When performing programming with FlashPro in the uPD78F0034A, what is the data in areas that are not programmed?

Answer:

The data in such areas is 0xFF.
Suitable Products
  • 이 기사가 도움이 되셨나요?