메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

What is the difference between the IE-78K0S-NS and the IE-78K0S-NS-A?

Latest Updated:12/01/2011

Question:

What is the difference between the IE-78K0S-NS and the IE-78K0S-NS-A?

Answer:

The IE-78K0S-NS features the addition of performance functions, and for this reason has been named IE-78K0S-NS-A.
Suitable Products
78K Family
  • 이 기사가 도움이 되셨나요?