메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

What is the method for enabling watchdog timer function?

Latest Updated:09/27/2004

Question:

(Watchdog Timer)   Watchdog timer function can be stopped by using continuous description of the DWDT and WRST instructions. What is the method for enabling watchdog timer function? [2004/09/27]

Answer:

Watchdog timer function is enabled at reset and return from RAM back-up mode or clock operating mode.
Also, disable interrupts (execute the DI instruction) when executing continuous instructions. (#105050)
Suitable Products
4508
4509
4559
455A
4571
  • 이 기사가 도움이 되셨나요?