메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

What is the oscillation settling time of the on-chip oscillator?

Latest Updated:05/24/2007

Question:

(Clock)  What is the oscillation settling time of the on-chip oscillator? [2007/05/24]

Answer:

When the MCU is used within the specified values, oscillation settling time is not required. (#106675)
Suitable Products
4508
4509
4559
455A
  • 이 기사가 도움이 되셨나요?