메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

What is the recommended screening (baking) time and temperature?

Latest Updated:10/19/2004

Question:

(Flash Memory)   What is the recommended screening (baking) time and temperature? [2004/10/19]

Answer:

Screening (baking) is not necessary after rewriting.
Suitable Products
3803H
3803L
3850A
38D2
  • 이 기사가 도움이 되셨나요?