메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

What is the starting voltage for RC oscillation?

Latest Updated:07/04/2003

Question:

(Electrical Characteristics)   What is the starting voltage for RC oscillation?

Answer:

Since RC oscillation is started by the execution of the CRCK instruction by a program after reset, use a voltage which falls within the RC oscillation power voltage shown in the recommended operating conditions. The recommended operating conditions are listed in the datasheet. (#105043)
Suitable Products
4508
4509
4559
  • 이 기사가 도움이 되셨나요?