메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

What to set memory mapping configuration box seen at debugger startup

Latest Updated:12/01/2011

Question:

What should be set for the memory mapping in the configuration dialog box displayed at debugger startup?

Answer:

This is an item specified when using a memory other than the internal memory of the device (when using externally connected memory, or when using ROM/RAM emulation memory in the ICE).
Nothing need be specified when using just the device's internal memory.
(Since the device's internal memory is automatically secured, setting memory that is redundant with this memory causes an error.)
Suitable Products
78K Family
  • 이 기사가 도움이 되셨나요?