메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

What units are used for reprogramming the Flash memory?

Latest Updated:03/01/2005

Question:

(Flash Memory)   The Flash memory is written to in byte units. What units are used for reprogramming? [2005/03/01]

Answer:

The erase unit determines the reprogramming unit for the flash memory, which is in this case is block units. (#104882)
Suitable Products
3803H
3803L
3850A
38D2
38D5
  • 이 기사가 도움이 되셨나요?