메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Which package of EIAJ, JEDEC, etc. is used for uPD789316GK-XXX-9ET ?

Latest Updated:12/01/2011

Question:

Which package of the following three types is used for the uPD789316GK-XXX-9ET ?

(1) EIAJ type
(2) JEDEC type
(3) Other

Answer:

(2) JEDEC type
Suitable Products
UPD78931x
  • 이 기사가 도움이 되셨나요?