메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Why does the direction register of any port have a protect register?

Latest Updated:03/15/2012

Question:

Why does the direction register of any port have a protect register?

Answer:

It is to prevent change of the value of the direction register caused by a runaway or others and improve the system reliability by allocating the port that has a protection register to important I/O.
Suitable Products
R8C/20
R8C/21
R8C/22
R8C/23
R8C/24
R8C/25
R8C/2A
R8C/2B
R8C/2C
R8C/2D
R8C/2E
R8C/2F
R8C/2G
R8C/2K
R8C/2L
R8C/33C
R8C/34C
R8C/35C
R8C/36C
R8C/38C
R8C/3GC
R8C/3JC
R8C/33D
R8C/35D
R8C/3GD
R8C/33T
R8C/38A
R8C/34E, R8C/34F, R8C/34G, R8C/34H
R8C/36E, R8C/36F, R8C/36G, R8C/36H
R8C/38E, R8C/38F, R8C/38G, R8C/38H
M32C/8A
M32C/88
M32C/87
M32C/85
M32C/84
M32C/83
M32C/80
M16C/62A
M16C/62A(M16C/62T)
M16C/62M
M16C/62N
M16C/62N(M3062GF8NFP, M3062GF8NGP)
M16C/62P
M16C/63
M16C/64A
M16C/64C
M16C/65
M16C/65C
M16C/6C
M16C/6N4, M16C/6N5
M16C/6NK, M16C/6NL, M16C/6NM, M16C/6NN
M16C/5L, M16C/56
M16C/5LD, M16C/56D
M16C/5M, M16C/57
M16C/30P
M16C/29
M16C/28
M16C/26A
M16C/1N
  • 이 기사가 도움이 되셨나요?