메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Will the WDT resets if it the entire LSI resets internally?

Latest Updated:03/26/2009

Question:

The hardware manual states that if WDT overflows, the entire LSI are reset internally. In this case, is the WDT also reset?

Answer:

With the internal oscillator, setting overflow time is made independently from the system clock and sub-clock. The time to the generation of internal reset by counting up from 0 to 255 is 0.2-typ0.4sec.
Suitable Products
H8/300H Tiny
H8/36109
H8/36087
H8/36077, H8/36079
H8/36064
H8/36049
H8/36037, H8/36057
H8/36014, H8/36024
H8/3694
H8/3687
H8/3672
H8/3664
H8/36912, H8/36902
  • 이 기사가 도움이 되셨나요?