메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Can I use licenses for Standard and Professional editions of revisions before the licenses were divided?

Last Updated:05/17/2017

Question:

Is it possible to use licenses for Standard and Professional editions of revisions before the licenses were divided in this way?

Answer:

Yes, you can use either license for old revisions.
Suitable Products
C Compiler Package for RH850 Family
C/C++ Compiler Package for RX Family
C Compiler Package for RL78 Family
  • 이 기사가 도움이 되셨나요?