메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Comparison of CRC result_CC-RL

Last Updated:02/07/2018

Question:

I am using RL78 compiler CC-RL.
The CRC result of MCU does not match to the value calculated by the linker in a program. The value calculated by the linker is stored in address 0x1fffc and matches to the CRC result of MCU on a debug tool. Can you tell me a probable cause for this?

Answer:

Access the area with the far attribute pointer since address 0x1fffc in which the CRC result calculated by the linker is stored is not the mirror area of the MCU.
Note that the near attribute pointer cannot access addresses other than the mirror area.

Suitable Products

e² studio
CS+ (formerly CubeSuite+)
C Compiler Package for RL78 Family
  • 이 기사가 도움이 되셨나요?