메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Difference between the Standard and Professional editions

Last Updated:05/17/2017

Question:

What is the difference between the Standard and Professional editions?

Answer:

The C language specifications of the Standard editions comply with the ANSI standard and it provides the essential features needed to write embedded programs. We will continue to enhance compiler optimization in relation to the efficiency of code and performance in the Standard editions.

We provide additional features which help to obtain even higher quality for the customer’s programs and shorten development periods in the Professional editions. The additional features will continue to be improved as we upgrade the products by producing new revisions.

Suitable Products
C Compiler Package for RH850 Family
C/C++ Compiler Package for RX Family
C Compiler Package for RL78 Family
  • 이 기사가 도움이 되셨나요?