메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

E0562300 message_CC-RH_CC-RX_CC-RL

Last Updated:09/20/2017

Question:

I am using Renesas Compiler. The following error message appears. How do I resolve this?

E0562300:Duplicate symbol "symbol-name" in "file-name"

Answer:

Because the same symbol is defined in multiple files, the message is output.

Confirm that the symbol output in the message is not defined in files (including included files) other than the source file corresponding to *.obj that was output in the message.
For different uses, change the symbol to a different symbol.
For the same use, add the extern storage class specifier to a location other than the definition area.

Suitable Products
e² studio
CS+ (formerly CubeSuite+)
C Compiler Package for RL78 Family
C Compiler Package for RH850 Family
C/C++ Compiler Package for RX Family
  • 이 기사가 도움이 되셨나요?