메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Is there any difference in compilers to be used between when using Node locked license and when using Floating license

Last Updated:03/16/2017

Question:

Is there any difference in compilers to be used between when using Node locked license and when using Floating license?

Answer:

No. You can start up the same compiler with whichever license you have.
Suitable Products
C Compiler Package for RH850 Family
C/C++ Compiler Package for RX Family
C Compiler Package for RL78 Family