메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

W0511180 Message(CC-RL)

Last Updated:06/07/2017

Question:

I am using RL78 compiler CC-RL. How do I resolve the “W0511180: The evaluation period has expired.” error?

Answer:

The error message appears when 60 days or more have passed since the first build for CC-RL V1.xx.xx and the evaluation period for the evaluation edition has expired.

If you have the commercial edition of the compiler, register its license key via license manager.

Suitable Products
e² studio
CS+ (formerly CubeSuite+)
C Compiler Package for RL78 Family
  • 이 기사가 도움이 되셨나요?