메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

W2000001 Message_CC-RL/CC-RX/CC-RH

Last Updated:12/06/2017

Question:

The following error message appeared. How do I resolve this?
"The function xxx cannot be found. (W2000001)"

Answer:

[Workaround] Check whether the function of the function name located at the cursor position exists in the project.

Output the cross reference information and confirm that build has been completed.
(When the function name is displayed in the function list, the cross reference information should normally be output.)

See also “CS+ Integrated Development Environment User’s Manual: Message” for your reference.
 

Suitable Products
C Compiler Package for RL78 Family
C Compiler Package for RH850 Family
C/C++ Compiler Package for RX Family
RL78 Family
RH850 Family
RX Family
  • 이 기사가 도움이 되셨나요?