메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

What causes this non-map error and what is the countermeasure?

Last Updated: 11/14/2017

Question:

A non-map break occurs in the debugger and the program execution stops. No error in particular occurs in the compiler and linker. What causes this non-map error and what is the countermeasure?

Answer:

It is not possible to tell based solely on this information. If a non-map break occurs and program execution stops, that the data used to access problematic non-mapped areas should remain in the trace data. Please check whether this is really access to memory other than the relevant memory.
Suitable Products
78K Family
  • 이 기사가 도움이 되셨나요?