메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

What should I install to build environment with Floating License?

Last Updated:06/28/2017

Question:

What should I install to build an environment with a floating license?

Answer:

Install the floating license management software in a server PC and the compiler and license manager in a client PC.

After installation, specify the IP address of the server PC in the license manager settings.

Suitable Products
C Compiler Package for RH850 Family
C/C++ Compiler Package for RX Family
C Compiler Package for RL78 Family
  • 이 기사가 도움이 되셨나요?