메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

"Please teach me how to output objects in the binary format. "

Latest Updated:10/28/2014

Question:

I am using CubeSuite+ for RL78, 78K and V850.
I was able to output objects in the hex format or Motorola S type format using the object converter of the build tool. Please teach me how to output objects in the binary format.

Answer:

The build tool of CubeSuite+ for RL78, 78K and V850 does not have a function to output objects in the binary format.

Note however that the memory contents of the debug tool currently connected can be saved (uploaded) in an arbitrary file in the binary format using the following method.

  • From the [Debug] menu, select [Upload…].
  • In the [Data Save] dialog box, specify an arbitrary file in [File Name], select "Binary data (*.bin)" in [File Type], and specify the range of addresses to save in [Save Range Address/Symbol].
  • Click the [Save] button to save the memory contents as upload data.

For details, refer to the following manual from here.
Section 2.5.3, Execute uploading, in CubeSuite+ Integrated Development Environment User's Manual: Debug

Suitable Products
CS+ (formerly CubeSuite+)
C Compiler Package for V850 Family
Compiler Package for V850 [CA850]
C Compiler Package for RL78 and 78K Families
Compiler for RL78 Family and 78K0R [CA78K0R]
E1 [R0E000010KCE00]
E20 [R0E000200KCT00]