메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Can I purchase user interface cable for E10A-USB emulator?

Latest Updated:10/28/2009

Question:

Can I purchase user interface cable for E10A-USB emulator additionally?

Answer:

Yes, you can. We provide 14pin, 36pin, and 38pin cable individually. Please refer to here for details of each cable and product No.
Suitable Products
E10A-USB
HS0005KCU01H
HS0005KCU02H