메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Can I use the AUD function if I purchase a 36-pin cable separately?

Latest Updated:05/30/2007

Question:

I have an E10A-USB (HS0005KCU01H) that does not include the AUD function. Can I use the AUD function if I purchase a 36-pin cable separately?

Answer:

No, the AUD function on E10A-USB (HS0005KCU01H) can't be used.
Because the circuit in the E10A-USB unit does not include a function for obtaining information from the AUD signal, you won't be able to use the AUD function even by connecting a 36-pin cable.
Suitable Products
E10A-USB