메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Do all block addresses of memory need to input in external flash memory?

Latest Updated:03/14/2008

Question:

I am currently using the H8S/H8SX external flash memory write function.
Do all block addresses of the Flash memory need to be input in "Top address of block" in the [External Flash memory setting] dialog even when not all of the Flash memory area is being used?

Answer:

Only input the addresses of the actual blocks you will be using in "Top address of block". Also, in the "block count", input the number of block addresses you input in "Top address of block."

Suitable Products
E10A-USB