메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Error message-set point not ram-when setting software break

Last Updated:09/27/2017

Question:

I am trying to set a software break but I get the "set point not ram" message.

Answer:

This error is displayed when the target memory is not set to the RAM or the RAM cannot be read/written.
Confirm the following items:

Make sure the target memory is set to the RAM.
Make sure the target memory area is opened in the memory window and read/write is enabled in this area.
If read/write still cannot be performed, check the BSC register setting. If the target memory is set to the SDRAM, the SDRAM must be initialized before setting the software break.

Suitable Products

E10A-USB
E200F
  • 이 기사가 도움이 되셨나요?