메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

How to retrieve an ID code when using the E1, E20, E8a or E8(discontinued product)

Last Updated:04/26/2017

Question:

Are there any methods for retrieving an ID code when using On-Chip Debugging Emulator the E1, E20, E8a or E8(discontinued product) (applies to M16C, incl. R32C, and R8C Family MCUs)?

Answer:

In some cases, the ID code can be retrieved. Refer to the following instructions.

Instructions : M16C_APN_ID_110607e.pdf(332KB)

Refer to the following FAQ for the specification of the ID code.

FAQ No. Suitable Emulator Description
106887 E1, E20, E8a How to handle ID codes
106937 E8 (discontinued product) How to handle ID codes
101717 E1, E20, E8a
E8 (discontinued product)
E7 (discontinued product)
What should I enter in the dialog box asking for an ID code?
106426 E1, E20, E8a
E8 (discontinued product)
ID code error appears
Suitable Products
E1 [R0E000010KCE00]
E20 [R0E000200KCT00]
E8a
E8
  • 이 기사가 도움이 되셨나요?