메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

How to write without reading to I/O register_HEW

Latest Updated:10/11/2017

Question:

When I try to write to the I/O register in the HEW memory window or I/O register window, read is also automatically performed. Is there any way to write to the register without reading it?

Answer:

Open the command line window by going to the HEW menu bar and selecting [Display] -> [Command Line].
By using the command described below you can write to the I/O register without initiating a read.
(However, when using E8/E8a emulators, this is only effective for the H8 Family.)
Command: hdi memwrite
This command writes data to the target system memory.

Syntax:
hdi memwrite space address size data
Functions for the hdi memwrite command is as follows:
Space: specify the address of the space to be used. This is only for processors that have multiple address spaces. For single address space processors, specify "0".
Address: address of first data to be written.
Size: size of data to be written; 1 = byte, 2 = word, 4 = long word
Data: data to be written; A successful write will return an empty character string. An error will return an error character string.

Example:
hdi memwrite 0 ff00 1 ff
(when writing byte-data H'FF to address H'FF00)

Note:
If the target address is displayed in the memory window or I/O register window at this point, a read event has occurred.

Suitable Products

HS0005KCU01H
HS0005KCU02H
  • 이 기사가 도움이 되셨나요?