메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Information about RX family MCUs with E1/E20 emulator and the HEW

Latest Updated:04/26/2017

Question:

It is my first time to develop an application using RX family MCUs with E1/E20 emulator and the High-performance Embedded Workshop.
Can you tell me which documents will help me? Are there any information as references?

Answer:

Refer to the following.

  Name of References References Reference Sections Descriptions
Basic
Operations
E1/E20 Emulator Additional Document for User's Manual E1 E20 Section 3 Preparations for Debugging
Section 6 Tutorial
From activation the High-performance Embedded Workshop to basic debugging operations with the E1/E20 emulator.
The tutorial program is designed to help users to understand how to use the functions of the emulator and emulator
debugger.
E1 On-Chip Debugging Emulator Application Note Introductory Guide for the RX610 Group E1 3. Installation
4. Let's Try Using the E1 Emulator
This introductory guide is intended for first-time users of the E1 emulator and provides simple instructions.
Debugger
Functions
E1/E20 Emulator Additional Document for User's Manual E1 E20 Section 5 Emulator Functions The emulator functions the E1/E20 emulator supports
High-performance Embedded Workshop User's Manual E1/E20 17. Debugging Facility Common functions of emulator products operated under the High-performance Embedded Workshop.
[Emulator Help] in the High-performance Embedded Workshop [Help] menu - The E1/E20 emulator functions +
The emulator functions on RX family MCUs.
 [Help Topic] in the High-performance Embedded Workshop [Help] menu -   - Common functions of emulator products operated under the High-performance Embedded Workshop.
Troubleshootings E1/E20 Emulator User's Manual E1 E20 3. Troubleshooting (Action in Case of an Error) How to solve a trouble when any problem occurs before the emulator debugger starts after the emulator and the user system have been powered on.
E1/E20 Emulator Additional Document for User's Manual E1 E20 Section 7 Notes on Usage Restrictions on using the E1/E20 emulator
On-Chip Debugging Emulator E1/E20 Troubleshooting Guide (for the RX600 Series) E1 E20 1. Troubleshooting on Startup
2. Troubleshooting in Operations after Startup
This document gives examples of problems and remedies for these problems for user debugging with RX600-series MCUs.
FAQ E1 E20 - The faq page for E1/E20 emulator
FAQ List of troubleshootings E1/E20 - The FAQ portal site of the common question when using the E1/E20 emulator
FAQ List of error messages E1/E20 - The FAQ portal site of the error message that E1/E20 emulator outputs
Fault E1/E20 Emulator User's Manual E1 E20 Appendix A Self-Checking Program (SCP) The procedure for using the self-checking program for the E1 and E20 in fault analysis.
Latest
Information
Tool News E1 E20 - Information about the upgraded versions, the precautions and etc.
Etc. External Flash Definition Editor User's Manual E1 E20 - Introductory guide for the utility software "External Flash Definition Editor" that create the definition files to write to an external flash memory by GUI operations easily.
External Flash Definition Editor Application Note Creating a Custom Program E1 E20 - A summary of the procedure for creating a custom program that is specifiable in the External Flash Definition Editor
FAQ List of know-how E1/E20 - The FAQ portal site which know-how on using the E1/E20 emulator is summarized
Suitable Products
E1 [R0E000010KCE00]
E20 [R0E000200KCT00]