메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Use of E8/E8a emulator in English OS on PC

Last Updated:10/18/2017

Question:

Can the E8/E8a Emulator be used on a computer that runs on an English OS?

Answer:

It can be used.
When the High-performance Embedded Workshop or the E8/E8a emulator software is installed to a personal computer equipped with an English OS, the English environment will automatically be installed (documents, help file, display, etc.).

Suitable Products

E8
E8a
  • 이 기사가 도움이 되셨나요?