메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Use of old compiler packages in E8a_E8_E7

Last Updated:10/18/2017

Question:

Can I use old compiler packages in the E8a, E8 or E7 emulator?

Answer:

In use of the microcomputer for H8 family, the data form which be downloaded by E8a, E8 or E7 emulator has the four following kinds.

  • ELF/DWARF2(.abs with debug information)
  • S-Record (.mot Motorola format)
  • Binary
  • Intel Hex

In order to debug with a source code, it is necessary to download a program in the form of ELF/DWARF2. In this case, please use Ver4.0 (C / C++ compiler Ver4.0 or later, Hew1.2 or later) or later of the compiler package for H8 family.

If you would like to use compiler version 4.0 or prior, since a file with debugging information (.abs) is SYSROF form, it cannot be downloaded by E8a, E8 or E7 emulator. Please specify the file format as S-Record, Binary, or Intel Hex form, and then download it.

How to output S-Record, Binary, and Intel Hex form

Please specify the following in the output file format of linkage editor.

  • S-type via absolute
  • HEX via absolute
  • Binary via absolute

Please refer to E7-f1 about the installation method in the case of using Ver4.0 or later version.

Suitable Products

E7
E8
E8a
C/C++ Compiler Package for H8SX, H8S, H8 Family
  • 이 기사가 도움이 되셨나요?