메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Build Error When Including iodefine.h in RI850V4 V2 Sample Project for CS+

Last Updated:02/21/2018

Question:

When including iodefine.h in the sample project for RI850V4 V2 (for CS+), a build error occurred. How do I resolve this?

Answer:

In the [I/O header file generation option] tab of the [CC-RH (Build tool)] property, change the setting as follows.

    [Output definition in consideration of μITRON] : 
    [No] -> [Yes (-uitron=on) ]
    [Update I/O header files during building] : 
    [Yes (select the device files only)] -> [Yes (select the device files and property)]
 

Suitable Products

RI850V4V2
  • 이 기사가 도움이 되셨나요?