메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Is it okay to set valid or invalid for protection under IR600PX system?

Latest Updated:09/04/2015

Question:

Is it possible to set “valid” or “invalid” for memory protection under the IR600PX operating system?

Answer:

Memory protection can be defined is units of “domain” for up to 15 objects.

When all 15 memory objects are settled in their respective domains, protection for each can be enabled or disabled. Enabling and disabling can be set for all memory objects at once by only defining a single domain to which all of the memory objects belong.

Suitable Products
RI600PX Real-time OS for RX Family