메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Uninstalling the RTOS Plug-in

Last Updated:05/31/2017

Question:

I am using the RI78V4 V2 package. (I was using it.)

I uninstalled the RTOS Plug-in, but cannot delete the related files. How do I resolve this?

Answer:

Please uninstall after installing the real-time OS common plug-in using the following standalone installer.

CSPlus_CC_Realtime_OS_Common_Plugins__V30100.exe 

Suitable Products

RI78V4 V2 Real-time OS for RL78 Family

  • 이 기사가 도움이 되셨나요?