메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

What are the INT numbers of interrupts used by the RI600V4 OS?

Latest Updated:11/10/2015

Question:

What are the INT numbers of interrupts used by the RI600V4 OS?

Answer:

The INT numbers are from 1 to 8.

Suitable Products
RI600V4 Real-time OS for RX Family
  • 이 기사가 도움이 되셨나요?