메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

"Warning message may appear when generating standard library file. "

Latest Updated:09/10/2007

Question:

I use SHC Compiler. [L1200(W) Backed up file "a.lib" into "b.lbk"] may be displayed when generating a standard library file.

Answer:

This is just a warning message that HEW will backup the old library file before generating a new library file.

Doing the followings will make this warning message undisplayed.

  1. Select [SuperH RISC engine Standard Toolchain...] from Options menu in the HEW.

  2. Select [Mode] from Category in [Standard Library] tab window.

  3. Select [Build a library file(option changed)] in Mode drop down list.

Suitable Products
C/C++ Compiler Package for SuperH Family