메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

An error showed when using the following link directive for the LK78K4.

Latest Updated:12/01/2011

Question:

An error is output during linking using the following link directive for the LK78K4.

  memory ROM :(0, 0EE00H)
  memory RAM :(0EE00H, 1100H)

Answer:

There is a problem with the RAM area definition.
In the 78K4, the RAM must always include the SFR area.
In the inquiry settings, definition is done only until immediately before the SFR area.
Change the RAM size from 1100h to 1200h.
This problem is believed to cause the F111 error, and subsequently the F304 error.
Suitable Products
  • 이 기사가 도움이 되셨나요?