메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Applilet2 does not work on Windows 7

Last Updated:08/02/2017

Question:

After I migrated from Windows XP to Windows 7, Appliet2 for xx does not work.

Answer:

Applilet2 creates temp files for operation in the Program Files folder of Windows. Since writing in the Program Files folder is prohibited in Windows 7 and later, Applilet2 does not work. Search by “windows 7 programfiles authority”, and change the administrator authority of the Program Files\NEC Electronics Tools folder or below, then change to the log-on user.
Suitable Products
Code Generator
  • 이 기사가 도움이 되셨나요?