메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Are there recommended interval to execute EEL_Handler?

Latest Updated:04/23/2014

Question:

In the libraries for the RL78 below, is there any recommended interval for executing the EEL_Handler function while the EEL_Execute function is running?

  • EEPROM Emulation Library Pack01
  • EEPROM Emulation Library Pack02

Answer:

There is no recommended interval for executing the EEL_Handler function.
To suppress effects of the interval for calling the EEL_Handler function on the processing time of the EEL_Execute function, we recommend continuously executing the EEL_Handler function.
Suitable Products
Data Flash Libraries
  • 이 기사가 도움이 되셨나요?