메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Are those lines displayed on window of IO Wizard represents output?

Latest Updated:09/04/2009

Question:

Are those program lines displayed on status window of IO Wizard during peripheral settings representing the program lines generated on the output .c file ?

Answer:

Yes, all program lines displayed on status window will be generated on the output ,c file. However, the order of program lines shown in status window and program lines generated on the output .c file might not be the same.
Suitable Products
 
  • 이 기사가 도움이 되셨나요?