메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Can IO Wizard insert source codes into multiple HEW workspace at one go?

Latest Updated:09/04/2009

Question:

Can IO Wizard insert source codes into multiple HEW workspaces at one go?

Answer:

IO Wizard is designed to insert source code into the current active HEW workspace. As such, please ensure that only 1 copy of HEW is opened when IO Wizard is to be used.
Suitable Products
  • 이 기사가 도움이 되셨나요?