메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Can I ask Renesas to prepare the mask file generation?

Latest Updated:09/15/2006

Question:

Even if I do not know the part name yet, can I ask Renesas to prepare the mask file generation?

Answer:

Please contact your Renesas Rep. or sales office for the ROM number.
We do not handle customer mask file generation as a regular procedure. It is customary for the mask file generation to be completed by the customer.
Suitable Products
Maskfile Converter
4500 Series ROM Ordering
720 Series ROM Ordering
38000 Series ROM Ordering
740/7450/7470 Series ROM Ordering
7600 Series ROM Ordering
7200 Series ROM Ordering
7770 Series ROM Ordering
M16C Family ROM Ordering
R8C Family ROM Programmed Shipment Ordering
QzROM Programmed Shipment Ordering
ASSP ROM Ordering
OSD Controller ROM Ordering
  • 이 기사가 도움이 되셨나요?