메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Can capacity of RL78 family be kept small?

Latest Updated:02/18/2013

Question:

It is written in the manual of data flash library type 04 for the RL78 family that the data buffer capacity should be from 0 to 1024 bytes. Can this capacity be kept small?

Answer:

The data buffer capacity can be kept small by the usage method of the user because the data buffer capacity written in the manual is the RAM area for storing data to be written to or read from data flash memory.
Suitable Products
Data Flash Libraries